Improve error handling in case of AES issue
ID: LPCBARESDK-492
Status: Open
First reported: 6.0.14.1114
Fixed in: TBD
Description
For applications using the DA14585 in central mode, which use the AES engine for application layer encryption, the event requesting the encryption might get stuck. As a result the device will not enter sleep anymore.
Workaround
Running in production mode with the Watchdog reset enabled guarantees the device recovery.