1. Introduction
1.1. Before We Start
Before you start you need to:
Install the latest Smartsnippets Studio
Download the latest SDK for the DA1469x platforms
These can be downloaded from the DA1469x product page.
Additionally, for this tutorial a Pro Development kit is required.
The key goals of this tutorial are to:
Start working with a customized project
Analyze the key points of the code structure
Prepare both hardware and software to run a demonstration code example