5. Code Overview
5.1. Header Files
In main.c
file, add the following header file:
#include "hw_pdc.h"
#include "hw_wkup.h"
#include "hw_sys.h"
5.2. Application Task
In main.c
file, replace the prvTemplateTask
apllication task with the following code:
/* LED D1 status */
PRIVILEGED_DATA volatile static bool LED_status = 0;
/**
* @brief Template task increases a counter every mainCOUNTER_FREQUENCY_MS ms
*/
static void prvTemplateTask( void *pvParameters )
{
OS_TICK_TIME xNextWakeTime;
static uint32_t test_counter=0;
/* Initialise xNextWakeTime - this only needs to be done once. */
xNextWakeTime = OS_GET_TICK_COUNT();
for ( ;; ) {
/* Place this task in the blocked state until it is time to run again.
The block time is specified in ticks, the constant used converts ticks
to ms. While in the Blocked state this task will not consume any CPU
time. */
vTaskDelayUntil( &xNextWakeTime, mainCOUNTER_FREQUENCY_MS );
test_counter++;
/* Enable the COM power domain before handling any GPIO pin */
hw_sys_pd_com_enable();
hw_gpio_configure_pin(LED1_PORT, LED1_PIN, LED1_MODE, LED1_FUNC,
LED_status);
hw_gpio_pad_latch_enable (LED1_PORT, LED1_PIN);
hw_gpio_pad_latch_disable(LED1_PORT, LED1_PIN); /* Lock pin status */
/* Disable the COM power domain after handling the GPIO pins */
hw_sys_pd_com_disable();
if (test_counter % (1000 / OS_TICKS_2_MS(mainCOUNTER_FREQUENCY_MS))
== 0) {
printf("#");
fflush(stdout);
}
}
}
5.3. Wake-Up Timer Code
In main.c
file and after prvTemplateTask()
, add the following code used for handling external events via the wake-up controller:
/* WKUP KEY interrupt handler */
static void wkup_cb(void)
{
/* Clear the WKUP interrupt flag!!! */
hw_wkup_reset_interrupt();
/*
* Avoid using printf() within ISR context!!! It may crash your code.
* Instead, use notifications to notify a task to perform an action!!
*/
/* Toggle the led status */
LED_status_flag ^= 1;
}
/* Initialize the WKUP controller */
static void wkup_init(void)
{
/* Initialize the WKUP controller */
hw_wkup_init(NULL);
/*
* Set debounce time expressed in ms. Maximum allowable value is 63 ms.
* A value set to 0 disables the debounce functionality.
*/
hw_wkup_set_debounce_time(10);
/*
* Enable interrupts produced by the KEY block of the wakeup controller (debounce
* circuitry) and register a callback function to hit following a KEY event.
*/
hw_wkup_register_key_interrupt(wkup_cb, 1);
/*
* Set the polarity (rising/falling edge) that triggers the WKUP controller.
*
* \note The polarity is applied both to KEY and GPIO blocks of the controller
*
*/
hw_wkup_configure_pin(KEY1_PORT, KEY1_PIN, 1, HW_WKUP_PIN_STATE_LOW);
/* Enable interrupts of WKUP controller */
hw_wkup_enable_irq();
}
5.4. Hardware Initialization
In main.c
file, replace the prvSetupHardware()
routine with the following code used for configuring the pins utilized by the wake-up controller.
/**
* @brief Hardware Initialization
*/
static void prvSetupHardware(void)
{
/*
* The IRQ produced by the KEY sub block of the wakeup controller (debounced
* IO IRQ) is multiplexed with other trigger sources (VBUS IRQ, SYS2CMAC IRQ,
* JTAG present) in a single PDC peripheral trigger ID
* (HW_PDC_PERIPH_TRIG_ID_COMBO).
*/
#if !defined(CONFIG_USE_BLE) && (!dg_configENABLE_DEBUGGER) && (!dg_configUSE_SYS_CHARGER)
uint32_t pdc_wkup_combo_id = hw_pdc_add_entry(HW_PDC_LUT_ENTRY_VAL(
HW_PDC_TRIG_SELECT_PERIPHERAL,
HW_PDC_PERIPH_TRIG_ID_COMBO,
HW_PDC_MASTER_CM33, 0));
OS_ASSERT(pdc_wkup_combo_id != HW_PDC_INVALID_LUT_INDEX);
/* */
hw_pdc_set_pending(pdc_wkup_combo_id);
hw_pdc_acknowledge(pdc_wkup_combo_id);
#endif
wkup_init();
/* Init hardware */
pm_system_init(periph_init);
/* Enable the COM power domain before handling any GPIO pin */
hw_sys_pd_com_enable();
/* Configure the KEY1 push button on Pro DevKit */
HW_GPIO_SET_PIN_FUNCTION(KEY1);
HW_GPIO_PAD_LATCH_ENABLE(KEY1);
/* Lock the mode of the target GPIO pin */
HW_GPIO_PAD_LATCH_DISABLE(KEY1);
/* Disable the COM power domain after handling the GPIO pins */
hw_sys_pd_com_disable();
}