8. Measurement Results
This chapter lists indicative results as observed while measuring the peripheral device for the use cases described in chapter 2.
All samples were collected one minute after powering up the device to allow ample time for the CMAC to utilize its power saving procedures to their fullest. The sample duration was one minute as well.
The Charge columns represent the charge spent throughout the entire sampling process. In a similar fashion, AVG Cur columns correspond to the average current and represent both the average current of sleep times and the times that the system is awake.
For measurements that involve BLE events of any kind, the measurements are slightly lower than the actual power consumption due to limitation of the power analyzer. It is not possible to capture accurately currents under 10 μA in a measurement that also contains currents over 100 μA.
8.1. Advertising
8.2. Connected (Peripheral Side)
For this section, only the peripheral was measured as it is the most common role for a developed device.
8.2.1. Keep Alive Packets
CONN Interval |
XTAL32K Avg Cur |
XTAL32K Charge |
RCX Avg Cur |
RCX Charge |
---|---|---|---|---|
30ms |
107.181 μΑ |
6.430 mC |
125.499 μΑ |
7.529 mC |
400ms |
19.020 μΑ |
1.141 mC |
22.138 μΑ |
1.328 mC |
2000ms |
12.480 μΑ |
0.748 mC |
14.928 μΑ |
0.895 mC |
4000ms |
11.673 μΑ |
0.700 mC |
14.038 μΑ |
0.842 mC |
8.2.2. Read 20 Bytes
CONN Interval |
XTAL32K Avg Cur |
XTAL32K Charge |
RCX Avg Cur |
RCX Charge |
---|---|---|---|---|
30ms |
335.937 μΑ |
20.156 mC |
365.034 μΑ |
21.902 mC |
400ms |
35.956 μΑ |
2.157 mC |
40.342 μΑ |
2.420 mC |
2000ms |
15.922 μΑ |
0.955 mC |
18.471 μΑ |
1.108 mC |
4000ms |
13.338 μΑ |
0.800 mC |
15.472 μΑ |
0.928 mC |
8.2.3. Write 20 Bytes
CONN Interval |
XTAL32K Avg Cur |
XTAL32K Charge |
RCX Avg Cur |
RCX Charge |
---|---|---|---|---|
30ms |
312.267 μΑ |
18.736 mC |
356.261 μΑ |
21.375 mC |
400ms |
34.142 μΑ |
2.048 mC |
39.263 μΑ |
2.355 mC |
2000ms |
15.620 μΑ |
0.937 mC |
18.377 μΑ |
1.100 mC |
4000ms |
13.199 μΑ |
0.791 mC |
15.802 μΑ |
0.948 mC |
8.2.4. Write No Response 20 Bytes No Notifications Enabled
CONN Interval |
XTAL32K Avg Cur |
XTAL32K Charge |
RCX Avg Cur |
RCX Charge |
---|---|---|---|---|
30ms |
359.844 μΑ |
21.590 mC |
401.550 μΑ |
24.092 mC |
400ms |
38.255 μΑ |
2.295 mC |
43.454 μΑ |
2.607 mC |
2000ms |
16.482 μΑ |
0.988 mC |
18.980 μΑ |
1.138 mC |
4000ms |
13.722 μΑ |
0.823 mC |
15.901 μΑ |
0.954 mC |
8.3. MTU Comparisons
8.3.1. Read 509 Bytes Characteristic MTU 65 (default)
CONN Interval |
XTAL32K Avg Cur |
XTAL32K Charge |
RCX Avg Cur |
RCX Charge |
---|---|---|---|---|
30ms |
275.177 μΑ |
16.510 mC |
302.645 μΑ |
18.158 mC |
400ms |
31.259 μΑ |
1.875 mC |
35.004 μΑ |
2.100 mC |
2000ms |
14.994 μΑ |
0.899 mC |
17.169 μΑ |
1.030 mC |
4000ms |
12.831 μΑ |
0.769 mC |
15.165 μΑ |
0.909 mC |