35. Working with multiple projects
SmartSnippets™ Toolbox framework allows the user to work on multiple Development Kits on the same laptop or PC by opening multiple SmartSnippets™ Toolbox applications, one for each DK. The following assumptions are made:
Each SmartSnippets™ Toolbox application instance should use a different project
Each instance should be associated with a different DK board connected to the laptop or PC via its own Virtual COM port pair.