24. Working with multiple tools¶
SmartSnippets™ Toolbox has been designed to help user achieve maximum productivity by allowing multiple tools be displayed on the screen at the same time. When working with multiple tools, user can:
- Modify the size of each tool frame
- Determine the exact location of each tool frame, by dragging the tool frame title bar and placing it at the upper, lower, left or right side of another tool frame
- Stack and un-stack tool frames, by dragging the tool frame title bar and placing it at the center of another tool frame
- Minimize a tool frame. User can make it visible again by clicking on the corresponding left-hand side toolbox button
- Maximize a tool frame and restore it to its previous size and location
Note
The tools provided by the framework depend on chip version selection. Different toolset is available if user selects a DA14580/581/583, DA14585/6 or a DA1468x chip family.
Every time the user closes the application, all layout-related data is stored and restored next time the application starts. To restore layout to default, user can press the button of the horizontal toolbar.