8. ConclusionΒΆ

This tutorial described various sleep modes available on the DA14531 and DA14585/586 and the ways to configure them, also describing the usage and significance of each of the modes. Using this information, the user can opt for whichever sleep mode suits the end application.

References:

  1. DA14531 datasheet

  2. DA14531 developemtn kit pro

  3. Small example describing hibernation mode use-cases hibernation example

  4. DA14585 datasheet