3. Terms and Definitions
BLE Bluetooth® Low Energy
COM Communication Port
EEPROM Electrically Erasable Programmable Memory
GPIO General Purpose Input/Output
HCI Host Controller Interface
HW Hardware
IDE Integrated Development Environment
IF Intermediate Frequency
LED Light Emitting Diode
LO Local Oscillator
OTP One Time Programmable
RF Radio frequency
RFIOp Radio frequency Input/Output
SDK Software Development Kit
SoC System on Chip
SPI Serial Peripheral Interface
SRAM Static Random Access Memory
SWD Serial Wire Debug
SW Software
UART Universal Asynchronous Receiver/Transmitter
USB Universal Serial Bus